Installation - Metasys - M4-SNE10502-0 - M4-SNE22002-0 - M4-SNE110L2-0 - M4-SNE11002-0 - Supervisory Device - Network Engine - 16.0

M4-SNE Installation Guide

Product
Document revision
N
Version
16.0
Revision date
2026-06-03
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-01647
Follow these guidelines when you install a network engine:
  • Transport the network engine in the original container to minimize vibration and shock damage to the network engine.
  • Verify that all the parts shipped with the network engine are present.
  • Do not drop the network engine or subject it to physical shock.
Important: Do not open the network engine housing for any reason. The network engine has no user-serviceable parts inside. Tamper-evident labels on the device caution installers, service technicians, building owners, and our RMA inspectors from unauthorized opening or tampering of the device.