Mounting the SNE in a panel - Metasys - M4-SNE10502-0 - M4-SNE22002-0 - M4-SNE110L2-0 - M4-SNE11002-0 - Supervisory Device - Network Engine - 16.0

M4-SNE Installation Guide

Product
Document revision
N
Version
16.0
Revision date
2026-06-03
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-01647

To mount the SNE in a panel, follow these requirements:

  • Mount the panel in accordance with the manufacturer’s instructions.
  • Mount the network engine in the panel following the guidelines in the Location considerations and Mounting sections of this document.