Use the holes in the three mounting clips for wall mount applications. To mount the SNE on a vertical surface, complete the following steps:
- Pull the bottom two mounting clips downwards to their extended positions.
- Mark mounting hole locations on the wall using the dimensions shown in Figure 1, or hold the bracket against the wall and mark the hole locations through the mounting clips. The screw holes on the network engine can accommodate M4 and #8 screws.
- Drill holes in the wall based on the locations marked in Step 2. Insert wall anchors for each hole if necessary.
- Hold the device in place, insert the
screws through the mounting clips and into the screw holes, and then carefully tighten all
screws. Important: Do not overtighten the mounting screws. Overtightening the screws can crack the network engine wall mount feet or housing.