To mount the DIN rail and the SNE, complete the following steps:
- Securely mount a 19.0 cm (7.5 in.) or longer section of 35 mm (1 1/8 in.) DIN rail in the required space.
- On the network engine, extend the two lower mounting clips.
-
Hang the top of the network engine to the DIN rail clip. Then
press the network engine against the DIN rail and hold in place while pushing up
on the lower mounting clips to secure the unit.
Figure 1. Network Engine secured with mounting clips in latched positions (rear view)