Supported firmware versions - Metasys - M4-SNE10502-0 - M4-SNE22002-0 - M4-SNE110L2-0 - M4-SNE11002-0 - Supervisory Device - Network Engine - 16.0

M4-SNE Installation Guide

Product
Document revision
N
Version
16.0
Revision date
2026-06-03
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-01647

All firmware versions of Metasys Releases 12.0.x and later are supported for the various SNE and SNC (SNx) models.

The following table lists the supported firmware versions of Metasys Release 10.1.x and 11.0.x for the various SNx models. You can load an SNx with a firmware version that is at or later than the releases listed in the following table. For example, if you have an SNExxxx1-x at Release 10.1.2.73, you can upgrade to Release 11.0.0.1717. Do not load a 10.1.x or 11.0.x firmware version that does not meet the criteria in the following table.

Table 1. SNE/SNC 10.1.x and 11.0.x supported releases

Models

Manufacturing date codes

Supported releases

10.1.x

11.0.x

M4-SNExxxx0-x

M4-SNCxxxx0-x

All 10.1.0.1757 or later 11.0.0.1717 or later

M4-SNExxxx1-x

M4-SNCxxxx1-x

Prior to RY12140 10.1.2.73 or later 11.0.0.1717 or later

M4-SNExxxx1-x

M4-SNCxxxx1-x

RY12140 and newer 10.1.5.135 or later 11.0.2.341 or later

M4-SNExxxx2-x

M4-SNCxxxx2-x

All 10.1.5.135 or later 11.0.2.341 or later
Note: You can find the date code sticker either on the side of the unit, or the underside of the unit. The date is also located on the shipping box label.