SNE capabilities - Metasys - LIT-1901126 - M4-SNE10502-0 - M4-SNE1050x-0 - M4-SNE11002-0 - M4-SNE1100x-0 - M4-SNE110L2-0 - M4-SNE110Lx-0 - M4-SNE22002-0 - M4-SNE22002-0G - M4-SNE2200x-0 - Supervisory Device - Network Engine - 13.0

M4-SNE Catalog Page

Product name
Network Engine
Document type
Catalog Page
Document number
LIT-1901126
Version
13.0
Revision date
2024-08-26
Product status
Active
Table 1. SNE series network engine details: SNE2200x, SNE1100x, SNE1050x, SNE110Lx
Features SNE2200x-0

SNE22002-0G 1

SNE1100x-0 SNE1050x-0 SNE110Lx-0 2
Communication interfaces
  • 1 Ethernet port 3
  • 2 RS-485 ports
  • 2 USB ports 4
  • 1 Ethernet port3
  • 1 RS-485 port
  • 2 USB ports4
Maximum number of child engines when acting as a Site Director 3 2 2 0
Maximum allowed devices across all integrations. For example, MS/TP+IP. Includes VND integrations and devices brought in through routers. 600 150 60 110
BACnet/IP maximum trunks 5 , 6 2 2 2 2
BACnet/IP maximum devices per trunk 200 100 50 10
BACnet/SC maximum trunks 6 1 1 1 1
BACnet/SC maximum devices per trunk 7 150 100 50 10
BACnet MS/TP maximum trunks 2 1 1 1
BACnet MS/TP maximum devices per trunk (Johnson Controls devices only)
Note: A repeater is required if more than 50 Johnson Controls devices are on the same trunk.
100 100 50 100
BACnet MS/TP maximum devices per trunk (with third party)
Note: A repeater is required if more than 32 devices are on the same trunk and some are third party.
64 64 50 64
N2 maximum trunks 2 1 1 N/A
Mapped N2 devices per trunk
Note: A repeater is required if more than 50 devices are on the same trunk.
100 100 50 N/A
LonWorks maximum trunks 1 1 1 N/A
LonWorks maximum devices 255 127 60 N/A
Remote Field Bus maximum trunks 6 3 3 N/A
Remote Field Bus maximum Johnson Controls Devices per bus 32 32 32 N/A
Remote Field Bus maximum devices per bus (with third-party devices) 16 16 16 N/A
Maximum objects in device 8 5000 2500 2500 2500
Supported type of parent server
  • ADS
  • ADX
  • OAS
  • ADS
  • ADX
  • ADS-Lite-E
  • OAS
  • ADS
  • ADX
  • ADS-Lite-E
  • OAS
ADS-Lite-A only
Supported integrations
  • BACnet/SC
  • BACnet/IP
    • Simplex® Fire Alarm Control Unit (FACU)
    • Cree® SmartCast® Lighting Control
    • Molex® Lighting Control
  • BACnet MS/TP Field Controller (FC) Bus
  • N2 Bus
    Note: The M4-SNE110Lx-0 model does not support the N2 Bus.
  • LonWorks® (requires USB to LON adapter)
    Note: The M4-SNE110Lx-0 model does not support the LonWorks network interface.
  • Modbus: Modbus TCP/IP on Ethernet and Modbus Remote Terminal Unit on RS-485
  • KNX IP
  • M-Bus
  • Tyco® C•CURE® 9000 and victor® Video Management
  • Zettler® Fire Panel with RS-232 adapter
  • OPC Unified Architecture (OPC UA)
  • MQ Telemetry Transport (MQTT)
Operating system Wind River® Linux LTS 19 (LTS=long-term support)
Microprocessor NXP i.MX6 DualLite processor
Memory Flash 2GB of DDR3 RAM and 16 GB of eMMC Flash
User interface Metasys UI
1 The letter G in a model's product code indicates that the model is the Buy American version.
2 These models are intended for use with the ADS-Lite-A servers (only) in Australia, China, Hong Kong, India, Indonesia, Japan, Korea, Malaysia, New Zealand, Philippines, Singapore, Taiwan, Thailand, Vietnam, and select branches within regions of Africa and the Middle East.
3 Second Ethernet port available with use of the ACC-USBETH-0 adapter.
4 Only the supported USB integration adapters function with the SNE. Other integration adapters that are not supported cannot function with the SNE.
5 Two Ethernet device connections include one integral Ethernet port and the USB to Ethernet adapter, ACC-USBETH-0, as the second Ethernet port. BACnet/SC is not supported at this time. The second BACnet/IP trunk is supported only at Release 13.0 and later.
6 Direct Ethernet connection only. USB to Ethernet adapter does not support BACnet/SC at this time.
7 Multiple IP integrations can be on an engine, including BACnet/IP and BACnet/SC, but this is limited by the maximum devices that can be mapped to a trunk. The total number of BACnet/IP or BACnet/SC devices that you can map is 150. You cannot map 150 IP and 150 SC devices at the same time because they use the same BACnet Integration object.
8 Suggested object limit for performance considerations.