Application documentation - Metasys - LIT-1901126 - M4-SNE10502-0 - M4-SNE1050x-0 - M4-SNE11002-0 - M4-SNE1100x-0 - M4-SNE110L2-0 - M4-SNE110Lx-0 - M4-SNE22002-0 - M4-SNE22002-0G - M4-SNE2200x-0 - Supervisory Device - M4-SNE Network Engine - 13.0

M4-SNE Catalog Page

Product
Document type
Catalog Page
Document number
LIT-1901126
Version
13.0
Revision date
2024-08-26
Product status
Active
Refer to the NAE85/M4-SNE/M4-SNC Product Bulletin (LIT-12013296) for important product application information. In addition, refer to the Metasys for Validated Environments on Metasys UI Product Bulletin (LIT-12014261) for information about which releases support MVE and which network control engines are supported as validated devices at facilities that require regulatory compliance.