Using the display keypad - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

Use the keypad to navigate the display menu options and select options within the display.

Figure 1. Display and keypad navigation
Table 1. Display keypad navigation controls
Callout Button Description
1 Back Use to return to the previous screen.
2 Left/Right Use to navigate to the left and right in the current view to change the selected item.
3 Up/Down Use to navigate up and down in the current view to change the selected item or menu option.
4 OK Use to make a selection or to navigate to a selected item, such as a menu option or point detail.
5 Menu Use to return to the Main Menu.