Procedure
Figure 1. Trend details graphical view
| Callout |
Description |
| 1 |
Name or description of the point with a
trend. |
| 2 |
The trend displaying values over
time. |
| 3 |
Current value. |
| 4 |
Current timestamp and value on the
trend. |
| 5 |
Select to view data from the last 24 hours in a tabular
format. |
| 6 |
Selectable time ranges for the trend. |
-
From the Main Menu, select Trends.
-
To view a trend, highlight the trend, and press OK.
-
To change the time range and view trends for last 24Hr, 12Hr,
6Hr, or 1Hr time period, press the Left or Right arrows to scroll through the time ranges.
Note: For each time range the display
supports a maximum of 72 samples. If a trend has more than 72 samples then
the chart displays 72 samples. For more information and examples, see the
example below.
-
To check the value at a particular timestamp, press the Up
arrow to highlight the trend graph, press OK, and press
the Left or Right arrows to scroll
through the graph.
-
To view trend data from the last 24 hours in a tabular format, select
List.
Figure 2. Trend details table view
The trend table shows data from the last 24 hours, with a maximum of 72
samples. The data shown in the trend table is unfiltered.
Example
Filtering samples on
the trend graph
The display can display a maximum of 72
samples on the trend graph. For the display to show all 72 samples without
aggregation, the maximum time that you can configure between sample creation is
shown below:
- 1 Hr: 50 seconds
- 6 Hr: 5 minutes
- 12 Hr: 10 minutes
- 24 Hr: 20 minutes
Depending on how often you configure the trend to
collect a sample, the display may filter out in-between samples if the 72 maximum
sample threshold is reached.
If you configure the trend to
collect a sample every 5 minutes over a 6 hour time range, the display shows the
maximum of 72 samples and does not aggregate any samples.
If
you configure the trend to collect a sample every minute over a 6 hour time range,
the display shows a sample point on the graph for each set of five samples.
If you configure the trend to collect a sample every minute over a
12 hour time range, the display shows a sample point on the graph for each set of
ten samples.