Display settings - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02
Table 1. Display settings
Setting Description Configurable from display Options Default setting
Backlight Intensity Use this setting to set the brightness of the screen. Yes Bright See footnote
Medium
Dim
Off
Backlight Timeout

CG series with onboard display: use this setting to control how long the display remains back-lit when there is no user activity before going dim.

DLK display: use this setting to control how long the display remains back-lit when there is no user activity before turning off.

SNC series with onboard display: not available.

Yes 1 minute
5 minutes
1 hour
8 hours
Idle Timeout Use this setting to select how long the display waits when there is no user activity before logging off the user. When an idle timeout occurs, the Home screen displays. The backlight on the CG series with on-board display and the DLK display will also dim or turn off. Yes 1 minute
5 minutes
15 minutes
30 minutes
1 hour
Date Format Use this setting to set the date format. Yes MM-DD-YY MM-DD-YY
MM-DD-YYYY
DD-MONTH-YYYY
DD-MONTH-YY
DD-MM-YY
DD-MM-YYYY
Time Format Use this setting to set the time format. Yes 12 MM 12 MM
12 MM SS
12 MM AMPM
12 MM SS AMPM
24 MM
24 MM SS
Language

Use this setting to view the language.

SNC Integral Display: English, ​Chinese Simplified, ​​Chines​e Traditional, ​​Czech, ​​​​Dutch, ​French, ​German, ​​Hungarian, ​Italian, ​​Japanese, ​​Korean, ​​Norwegian, ​​Polish, ​​Portuguese (Brazilian), ​​Russian, Spanish, ​Swedish, and ​Turkish

DLK0350 Display and CGx Integral Display: English, ​​​Czech, ​​​​Dutch, ​French, ​German, ​​Hungarian, ​Italian, ​​​​​​Norwegian, ​​Polish, ​​Portuguese (Brazilian), ​​Russian, Spanish, ​Swedish, and ​Turkish

No N/A See footnote2
Object Label Use this setting to select the label that is shown on the point tiles. If you choose Name, the point tiles show the Name attribute of the point. If you choose Description, the point tiles show the Description attribute of the point. Yes Name Name
Description
Firmware Update3 Use this setting to select the update options for the DLK display. The device is shipped with Auto set by default.

Auto: Automatically applies new firmware downloads from an equipment controller.

Manual: Requires manual intervention to apply new firmware downloads.

Disabled: Disables receiving any new firmware downloads.

Yes Auto Auto
Manual
Disabled
Firmware Version Use this setting to view the firmware version of the display. No N/A See footnote4
Point Display Mode5 Use this setting to switch the display to show local hardware points or software points on an SNC connected display.
Note: When Point Display Mode is changed on a DLK0350 connected to an SNC, the DLK0350 display shows a communication failure screen for a few seconds as the UI updates to the selected point type.
Yes Local Hardware IO Local Hardware IO
Software Interface IO
1 The default setting is the setting that you set in CCT when you download the application. Backlight Timeout, Backlight Intensity, and Idle Timeout default values are set based on value received from the application.
2 For equipment controllers, the default language is the language that you set in CCT. For an SNC, the default language is the language package that you have downloaded on the SNC.
3 The Firmware Update setting is only available on the DLK0350. The CGx Integral Display doesn't have this setting and is always set to Auto.
4 The default firmware version is the version that you have downloaded on the display.
5 Only available on the SNC with onboard display or a DLK when connected to an SNC.