Controller settings - Metasys - LIT-12013762 - M4-CGE09090-0H - M4-CGM09090-0H - M4-DLK0350-0 - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-04H - M4-SNC16122-0H - M4-SNC25151-04H - M4-SNC25151-0H - M4-SNC25152-04H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Brand
Metasys
Product name
Local Controller Display
Document type
User Guide
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02
Language
English
Table 1. Controller settings
Setting Description Example
Status Current status of the controller or engine. Operational
Description Description of the controller or engine. VAV CTRL/ACT/DP 3 UI 2 CO 3 BO
Object Name Object name of the controller or engine. CG-22
Model Name Model name of the controller or engine. M4-CVM03050-0
System Name System name defined in CCT for the controller application. Default State
Computer Name Computer name of the controller or engine. SNE00108D0BD0E4
Supervisory Device Computer name of the engine that the equipment controller is connected to. SNE00108D0BD0E4
Instance Number The Instance Number of the controller. 1
Firmware Version Version of the firmware stored in the controller. 11.0.0.1231
CPU Usage Number representing the current Central Processing Unit (CPU) usage in percent. 1.000000
IP Address IP address of the IP enabled controller or engine. 192.168.1.10
IP Subnet Mask IP Subnet Mask of the IP enabled controller or engine. 255.255.255.0
Gateway Gateway address of the IP enabled controller or engine. 192.168.1.1
Ethernet MAC Address Ethernet MAC address of the IP enabled controller or engine. 2C:54:91:88:C9:E3
Ethernet 1 Link Speed The speed of the Ethernet on Ethernet Port number 1 of the SNC. 100 Mbps
Ethernet 2 Link Speed The speed of the Ethernet on Ethernet Port number 2 of the SNC. 100 Mbps
IP Communication Mode Communications type configured on the IP enabled controller or engine. Dual SC and IP Mode
JCI SC Primary Hub URI Uniform Resource Identifier (URI) for the Primary Hub Function. Available if IP Communication Mode is set to Secure Connect Only or Dual SC and IP Mode. wss://10.109.177.64:1443/
JCI SC Failover Hub URI URI for the Failover Hub Function. Available if IP Communication Mode is set to Secure Connect Only or Dual SC and IP Mode.  
BBMD Enabled Is set to True if BACnet/IP Broadcast Management Device (BBMD) is configured. Available if IP Communication Mode is set to Ethernet IP Only or Dual SC and IP Mode. False
BACnet/IP UDP port BACnet UDP Port address. Available if IP Communication Mode is set to Ethernet IP Only Mode. 47808
Secure Port Number TCP port number the BACnet/SC Datalink binds to for secure websocket communication. Available if IP Communication Mode is set to Secure Connect Only or Dual SC and IP Mode. 1443
FCB MAC Address Number representing the MAC address assigned to the MS/TP enabled controller. 10
FCB Baud Rate Baud rate configured for communication on the MS/TP Bus of the MS/TP enabled controller.. Auto
Note: The Ethernet 1 Link Speed and Ethernet 2 Link Speed information settings are only available for the SNC and are not available on IP equipment controllers.
Note: At firmware version 11.0 of the display and later, the controller settings shown in Table 1 only appear on the display if they are applicable to the engine or controller the display is connected to.