Home - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02
The Home screen is the main screen that displays after the display starts up. The Home screen, Figure 1, displays the favorite points that you configure in the Idle Page folder in the display configuration. You can navigate to the Point Details screen for any of the points that are shown on this screen. You can also navigate to the Alarms screen from this page. The Home screen reappears when the idle timeout expires. For more information on the commands that are available, see Commanding points.
Figure 1. Home screen
Note: If no points are configured to the Idle Page, or the display is using the plug and play configuration, then "No objects configured for this page" is displayed under the Home screen.