Point types on display - Metasys - LIT-12013762 - M4-CGE09090-0H - M4-CGM09090-0H - M4-DLK0350-0 - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-04H - M4-SNC16122-0H - M4-SNC25151-04H - M4-SNC25151-0H - M4-SNC25152-04H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Brand
Metasys
Product name
Local Controller Display
Document type
User Guide
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02
Language
English

The CG series controllers with onboard display, the SNC controller with onboard display, and the DLK0350 display connected to any supported controller show the hardware points of the application by default. However, the SNC controller with onboard display, and the DLK0350 display connected to an SNC can show the software points if the user changes the Point Display Mode setting to display the software points of an SNC. The Point Display Mode setting can be found on display under Settings > Display Settings > Point Display Mode and the software points can be found under Programming > Local Application folder of an SNC using SCT or Metasys UI. For more information about the points supported by the SNC, refer to the SNC Commissioning Guide (LIT-12013295).