If the display object is not configured in the application, then the display shows all BACnet exposed application points. All of the available input and output points are located under Equipment Data > Inputs/Outputs page, and all AV, BV, and MV points are available under Equipment Data > Parameters page.
Note: If the application on an SNC has a NetSensor, then a DLK connected to an SNC, or the integral display on an SNC
shows all value points of the NetSensor under the
Inputs/Outputs, similar to the Local Hardware I/O folder of an SNC.