The Main Menu options are Home, Alarms, Overrides, Equipment Data, Trends, Settings, and Log On. You can navigate to different options from the Main Menu as shown in Figure 1 and described in Table 1.
Figure 1. Local controller display Main Menu
To navigate to a Main Menu option, complete the following steps:
- On the keypad, press Menu to display the Main Menu.
- Press the Up or Down arrows to highlight one of the Main Menu options.
- Press OK.
| Main Menu options | Description |
|---|---|
| Home | Displays the points that you configure in the Idle Page folder in the display configuration within CCT. These can be important points or frequently referenced input/output or parameter points. |
| Alarms | Displays the alarms for the points configured for the display. For
details about the alarm types supported, see Alarms. Note: If the display is not configured,
Alarms are displayed for the BACnet exposed points that have
Alarms configured.
|
| Overrides | Displays the points that are currently overridden or put out of service. |
| Equipment Data | Displays the Inputs/Outputs page, Parameters page, and any user defined pages for the device. |
| Trends | Displays the trends associated with points configured for display.
For details about the trend types supported, see Trends. Note: If the display is not configured,
Trends are displayed for the BACnet exposed points that have
Trends configured.
|
| Settings | Provides navigation to the sub-menus Display Settings and Controller Settings. |
| Log On | Displays the Log On screen for the display. Note: This menu option is
available only if you have configured authorization for the
display in CCT.
|