Display information - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

The local display organizes the objects and data based on the display configuration defined in the controller's application. The points that you configure for the display are shown, and alarms and trends that are associated with these points. You cannot modify the configuration of the points from the local display but you can do so with CCT. In CCT, you can customize the points that are shown in the display and change the order and groupings of the information. For more information about how to configure the data shown in the display, refer to the Controller Tool Help (LIT-12011147).

Note: If the display object is not configured in the application, then the display shows all BACnet exposed application points. For more information on how the display organizes the points by default, see Plug and play configuration.