Setting a point in service - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document type
User Guide
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

Procedure

To set a point in service, complete the following steps:

  1. Navigate to the point that you want to put back in service and press OK.
  2. Highlight the present value and press OK.
  3. From the Commanding menu, select In Service, and press OK.
  4. Review the details of the in service command and to confirm press OK.
    Note: If you click Cancel, the command screen closes, and you do not issue the command.