Releasing an override - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

Procedure

To release an override or temporary override, complete the following steps:

  1. Navigate to the point that you want to release and press OK.
  2. Highlight the present value and press OK.
  3. From the Commanding menu, select Release Override, and press OK.
  4. Review the details of the release override command and to confirm press OK.
    Note: If you click Cancel, the command screen closes, and you do not release the override.