Releasing all overrides and command priorities - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

Procedure

If you use the Release All command, you release all priorities from 3 to 5 and from 7 to 16. For example, the Override command is at priority 8 and the Adjust command is at priority 16. For more information about analog output commands, refer to Analog Output Commands section of the Metasys Site Management Portal Help User Guide.
Note: The Release All command does not release Min on/off at priority 6.

To release all overrides and command priorities, complete the following steps:

  1. Navigate to the point that you want to release and press OK.
  2. Highlight the present value and press OK.
  3. From the Commanding menu, select Release All, and press OK.
  4. Review the details of the release all command and to confirm press OK.
    Note: If you click Cancel, the command screen closes, and you do not release all the overrides.