Procedure
Note: You can only temporarily override a point on a
display connected to an SNC, or the SNC with integral display.
- Navigate to the point that you want to temporarily override and press OK.
- Highlight the present value and press OK.
- From the Commanding menu, select Temporary Override, and press OK.
- Enter a value using the keypad or select an override value for the point, select the Green Check Mark icon when complete, and press OK.
- Enter a time in hours using the keypad or select a time in hours from the list. If you enter a value using the keypad, select the Green Check Mark icon when complete, and press OK. If you select a time from the list, select Next, and press OK.
- Enter a time in minutes using the keypad or select a time in minutes from the list. If you enter a value using the keypad, select the Green Check Mark icon when complete and press OK. If you select a time from the list, select Next, and press OK.
-
Review the details of the temporary override
command and to confirm press OK.
Note: If you click Cancel, the command screen closes, and you do not issue the command.