Overriding a point temporarily - Metasys - LIT-12013762 - M4-CGE09090-0H - M4-CGM09090-0H - M4-DLK0350-0 - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-04H - M4-SNC16122-0H - M4-SNC25151-04H - M4-SNC25151-0H - M4-SNC25152-04H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Brand
Metasys
Product name
Local Controller Display
Document type
User Guide
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02
Language
English

Procedure

Note: You can only temporarily override a point on a display connected to an SNC, or the SNC with integral display.
  1. Navigate to the point that you want to temporarily override and press OK.
  2. Highlight the present value and press OK.
  3. From the Commanding menu, select Temporary Override, and press OK.
  4. Enter a value using the keypad or select an override value for the point, select the Green Check Mark icon when complete, and press OK.
  5. Enter a time in hours using the keypad or select a time in hours from the list. If you enter a value using the keypad, select the Green Check Mark icon when complete, and press OK. If you select a time from the list, select Next, and press OK.
  6. Enter a time in minutes using the keypad or select a time in minutes from the list. If you enter a value using the keypad, select the Green Check Mark icon when complete and press OK. If you select a time from the list, select Next, and press OK.
  7. Review the details of the temporary override command and to confirm press OK.
    Note: If you click Cancel, the command screen closes, and you do not issue the command.