Overriding a point - Metasys - LIT-12013762 - M4-CGE09090-0H - M4-CGM09090-0H - M4-DLK0350-0 - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-04H - M4-SNC16122-0H - M4-SNC25151-04H - M4-SNC25151-0H - M4-SNC25152-04H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Brand
Metasys
Product name
Local Controller Display
Document type
User Guide
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02
Language
English

Procedure

To override a point, complete the following steps:

  1. Navigate to the point that you want to override and press OK.
  2. Highlight the present value and press OK.
  3. From the Commanding menu, select Override, and press OK.
  4. Enter or select a value for the point.
  5. Choose from one of the following options:
    • Analog points: Select the Green Check Mark icon when complete and press OK.
    • Binary/Multi-state points: Select Save and press OK.
    Note: If you click Close, the command screen closes, and you do not issue the command. This is applicable only to Binary/Multi-state points.
  6. Review the details of the override command and to confirm press OK.
    Note: If you click Cancel, the command screen closes, and you do not issue the command.