Adjusting a point - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

Procedure

To adjust a point, complete the following steps:

  1. Navigate to the point that you want to adjust and press OK.
  2. Highlight the present value and press OK.
  3. From the Commanding menu, select Adjust, and press OK.
  4. Enter or select a new value for the point.
  5. Choose from one of the following options:
    • Analog points: Select the Green Check Mark icon when complete and press OK.
    • Binary/Multi-state points: Select Save and press OK.
    Note: If you click Close, the command screen closes, and you do not issue the command. This is applicable only to Binary/Multi-state points.
  6. Review the details of the adjust command and to confirm press OK.
    Note: If you click Cancel, the command screen closes, and you do not issue the command.