Default password - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

The DLK0350 display has a password set by default. When you connect to an IP controller with a display, the default password is CHGxxxx where xxxx is the last four digits of the MAC Address of the IP controller that the DLK is connected to. When you connect to an MS/TP or N2 device with a display, the default password is CHGxxxx where xxxx is the controller's address. For example, if the address of the controller is 10, then the password is CHG0010. The password is always seven characters long. You can change the default password from the display configuration in the CCT.