Applying new firmware to a display manually - Metasys - LIT-12013762 - M4-CGM09090-0H - M4-CGE09090-0H - M4-SNC16122-04H - M4-SNC25151-04H - M4-SNC16121-04H - M4-SNC16121-0H - M4-SNC16122-0H - M4-SNC25152-04H - M4-DLK0350-0 - M4-SNC25151-0H - M4-SNC25152-0H - Field Device - Local Controller Display - 13.0

Local Controller Display User Guide

Product
Controls > Field Controls > Local Controller Display
Document number
LIT-12013762
Document revision
Version
13.0
Revision date
2023-10-02

Procedure

For more information about firmware updates, see Table 1.

  1. From the Main Menu, select Settings > Display Settings > Firmware Update > Manual, and press OK.
  2. If a new firmware update is available, select Apply, and press OK when the Firmware Update Available message appears.
    Note: If there is no new firmware update available, the Firmware Update Not Available message appears. Select Cancel, and press OK or press Back to return to the previous screen. No Apply option appears when there is no firmware update available.