Launcher Overview - Metasys - LIT-12011783 - Software Tool - Launcher - 1.7

Launcher Installation Guide

Brand
Metasys
Product name
Launcher
Document type
Installation Guide
Document number
LIT-12011783
Version
1.7
Revision date
2018-12-17
Language
English

The Launcher software application lets you access any Metasys server or supervisory engine on the building network, regardless of its software version. The Launcher comes in two forms: the full Launcher or the Single Site Connection Launcher.

Figure 1. Full Launcher (left) and Single Site Connection Launcher (right)

You select the Launcher type when you download the application. See Detailed Procedures.

Key features of the Launcher include:

  • Support to launch any version of the Site Management Portal (SMP) user interface or SCT. Supported user interfaces include the ADS, ADX, ADS-Lite, ODS, SCT, NAE, NIE, and NCE.
    Note: For Release 5.2 or earlier, the specific Java® Runtime Environment (JRE) particular to the SMP or SCT software release is still required on the client computer.
  • Support for launching any website, including Metasys software products such as Ready Access Portal, the Metasys UI, and the Metasys Advanced Reporting System, as well as Google® and Yahoo!® websites among others.

The full version of the Launcher software is installed by any of three methods:

When you install the full version of the Launcher software, a separate folder to store the Metasys release software is created on your hard disk. This practice provides for an isolated, private version of the JRE required to run Metasys software. If you have installed multiple releases of Metasys software, a separate folder is created for each. The locations for this folder depend on which operating system (OS) and release of Launcher you are using:

For the default location for Launcher 1.3 and earlier:

Windows® 10, Windows 8.1, Windows 7, Windows Server® 2012 R2, or Windows Server 2008 R2 operating systems:

C:\Users\<username>\JohnsonControls.Launcher\resources

Apple® OS X® operating systems:

~\Users\<username>\JohnsonControls.Launcher\resources

For the default location for Launcher 1.4 and later:

Windows® 10, Windows 8.1, Windows 7, Windows Server® 2012 R2, or Windows Server 2012 R2 operating systems:

C:\ProgramData\Johnson Controls\Launcher\resources

Apple® OS X® operating systems:

~\Users\Shared\Johnson Controls\Launcher\resources

Note:

With Launcher 1.4 and later, you have the option to store data in either the default ProgramData folder or the private user's directory folder in the Windows operating systems and similar folders on Apple OS X operating systems.

The private user's directory locations for Launcher 1.4 and later:

Windows: C:\Users\<username>\Johnson Controls\Launcher\resources

Mac: ~\Users\<username>\Johnson Controls\Launcher\resources

You install the Single Site Connection version of the Launcher by manually downloading a copy of the MetasysResource.zip file to your computer. You then unzip the file to a publicly accessible location on the computer so that everyone who uses the computer has access to the program.

After you install Launcher for a particular Metasys system release, use the Launcher to access the Site Management Portal, supervisory engine, or SCT. If you use the web browser instead, the Launcher Download screen appears again. Do not reinstall Launcher.