Starting the Launcher - Metasys - LIT-12011783 - Software Tool - Launcher - 1.7

Launcher Installation Guide

Brand
Metasys
Product name
Launcher
Document type
Installation Guide
Document number
LIT-12011783
Version
1.7
Revision date
2018-12-17
Language
English
Note: These steps assume that you have previously installed or unzipped the Launcher application. If you have not, see Downloading and Installing or Upgrading the Launcher: Full Installation to a Windows OS or Downloading and Installing or Upgrading the Launcher: Single Site Connection.

To start the Launcher, double-click the Launcher icon. Or if you installed the full version of Launcher on a Windows OS, select Programs > Johnson Controls > Launcher . The appropriate Launcher screen appears (Figure 1 or Figure 2).

Figure 1. Launcher Screen: Full Installation

Figure 2. Launcher Screen: Single Site Connection

For a description of each Launcher screen and details on how to use the Launcher, refer to Launcher Tool Help (LIT-12011742). This document is also available within the Launcher application as a Help file by clicking the question mark (?) icon on the Main Launcher screen.