LIP overview - Metasys - LIT-12011793 - Software Application - Language Installation Program - 12.0

Language Installation Program Installation Guide

Brand
Metasys
Product name
Language Installation Program
Document type
Installation Guide
Document number
LIT-12011793
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

The LIP is a software tool that installs and removes a set of language resources on a Metasys platform to support multiple different languages. The tool changes the site default language for Metasys servers, Metasys software applications, and network engine. For applications that support multiple languages, the LIP sets the language choices in addition to the default language. In this way, users with a different language preference can log on to the system and see the product’s UI in their preferred language.

To view the products that the LIP supports, see the following table:

Table 1. Metasys servers, software applications, and network engines supported by LIP

Type of network engine or application

Supported products

Metasys server software

Application and Data Server (ADS and ADS-Lite)

Extended Application and Data Server (ADX)

Open Data Server (ODS)
Important: The latest available version of the ODS is Release 10.1. The ODS is not available for upgrade to Metasys Release 12.0.

Open Application Server (OAS)

Metasys Advanced Reporting System

NAE85/LCS85 Site Management Portal (SMP)

NIE89 Site Management Portal

Metasys software Applications

Graphic Generation Tool (GGT)

Metasys Export Utility

Metasys UI or Johnson Controls System Configuration Tool (JCT)

System Configuration Tool (SCT)

Metasys network engines

NAE55

NAE85/LCS85

SNC1612

SNC2515

SNE1100

SNE2200

SNE1050

NAE35
NIE39 NAE45
NIE49 NCE25
NIE29