Summary of changes - Metasys - LIT-12011793 - Software Application - Language Installation Program - 12.0

Language Installation Program Installation Guide

Product name
Language Installation Program
Document type
Installation Guide
Document number
LIT-12011793
Version
12.0
Revision date
2022-05-20
Product status
Active

The following information is new or revised:

  • Removed support for Microsoft Windows 8.1®.
  • Replaced references to Metasys UI Offline with Johnson Controls System Configuration Tool (JCT) throughout this document, as this tool was rebranded.
  • Removed support for Energy Essentials.
  • Removed support for Open Data Server (ODS)
  • The LIP tool is not FIPS 140-2 compliant. If you install LIP on a FIPS 140-2 compliant Site Director, you must uninstall LIP after you add the additional languages.
Note: For more information, see LIP system requirements.