Uninstalling the LIP tool - Metasys - LIT-12011793 - Software Application - Language Installation Program - 12.0

Language Installation Program Installation Guide

Brand
Metasys
Product name
Language Installation Program
Document type
Installation Guide
Document number
LIT-12011793
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

Procedure

  1. On the host computer, click Start > Control Panel > Programs > Programs and Features.
  2. Right-click the appropriate Metasys Language Installation Program x.x, where x.x lists the version number of the LIP. For example, Metasys Language Installation Program 6.0. Click Uninstall.
  3. On the Metasys Language Installation Program 6.0 Setup window, click Uninstall.
  4. When the uninstall is complete, click Finish.