Obtaining and installing language packs - Metasys - LIT-12011793 - Software Application - Language Installation Program - 12.0

Language Installation Program Installation Guide

Brand
Metasys
Product name
Language Installation Program
Document type
Installation Guide
Document number
LIT-12011793
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

Procedure

  1. Use a web browser to navigate to the License Portal.
  2. On the Software tab, locate the Language Packs product and select the Download icon in the Actions column.
  3. In the Download Software dialog box, select the version of language packs you need and click Next.
  4. Click the hyperlinks in the Product column to find and select the folders associated with the language packs you need.
  5. Click Download.
  6. Unzip and save the translated language pack in the same folder that the LIP Tool resides, which is C:\Program Files (x86)\Johnson Controls\LIP.

    For information about how to use the LIP tool, refer to the Language Installation Program Help (LIT-12011349) .