LIP and language pack compatibility - Metasys - LIT-12011793 - Software Application - Language Installation Program - 12.0

Language Installation Program Installation Guide

Brand
Metasys
Product name
Language Installation Program
Document type
Installation Guide
Document number
LIT-12011793
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

To obtain LIP and language pack compatibility for each release, use the following table.

Table 1. LIP and language pack compatibility
Software release LIP version Language pack version
Metasys 12.0 6.0.0.xxx 6.0.0.xxx
Metasys 11.0 5.0.0.319 5.0.0.335
Metasys 10.1 4.1.0.256 4.1.0.315
Metasys 10.0 4.0.0.183 4.0.0.257
Metasys 9.0 4.0.0.183

3.0.0.101

4.0.0.257

3.0.0.209

Metasys 8.1 4.0.0.183 4.0.0.257
Metasys 8.0 4.0.0.183 4.0.0.257
Metasys 7.0 4.0.0.183 4.0.0.257
Metasys 6.5.25 4.0.0.183 4.0.0.257
Metasys 6.5 4.0.0.183 4.0.0.257
Metasys 6.1 4.0.0.183 4.0.0.257
Metasys 6.0 4.0.0.183 4.0.0.257
Metasys 5.2/5.3 4.0.0.183 4.0.0.257
GGT 3.0.0.101 1.2 for GGT version 1.2

1.3 for GGT version 1.3

The language pack contains the necessary components for all Metasys servers, applications, and network engines. All language packs, including legacy LIP language packs are available on the License Portal.

Note: We cannot guarantee performance and translation quality when you use a newer LIP Tool with an older language pack, or when applied to an engine at an older Metasys release. For best results, ensure that the LIP Tool and language packs are from the same Metasys release.