Network engines - Metasys - LIT-12011349 - Software Application - Language Installation Program - 13.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
13.0
Revision date
2024-02-20
Product status
Active
Language
English

When users log on to a network engine directly, the UI displays the network engine default language. This process occurs even if users have different languages assigned to their profiles in the Metasys server. SNx network engines only support the network engine default language. Ensure that the Site Director and any SNx engines on the site use the same default language.

When you change the default language or locale for a network engine, such as an SNE, SNC, NAE, or NCE, the LIP copies the translated language files from your computer to the appropriate folder on the network engine. After you make the change and the engine restarts, the newly selected language then becomes the language that is presented to all users of that network engine. For instructions on how to change the default language or locale, see Changing the locale for a language on a network engine or Changing the default language on a network engine.