Johnson Controls System Configuration Tool (JCT) - Metasys - LIT-12011349 - Software Application - Language Installation Program - 13.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
13.0
Revision date
2024-02-20
Product status
Active
Language
English

When you add an additional language for JCT, restart the device that runs JCT. Be sure to plan for this temporary downtime because all users currently logged in to JCT are logged out during this process.

You can customize the language that displays in JCT for each user by with the Tools > User Profile menu. If a language is not selected from the User Profile menu, the Metasys UI uses the same default language as the server.

You must install the same languages in SCT that you plan to view in JCT.