LIP overview - Metasys - LIT-12011349 - Software Application - Language Installation Program - 13.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
13.0
Revision date
2024-02-20
Product status
Active
Language
English

LIP is a software tool that installs and removes a set of language resources to support multiple languages on a Metasys platform. The tool changes the site default language and locale for Metasys servers, Metasys software applications, and network engines. For applications that support multiple languages, the LIP sets the language choices in addition to the default language. In this way, users with a different language preference can log on to the system and see the product’s interface in their preferred language.

The LIP tool is compatible with Metasys Release 5.2 or later.

Note: The LIP tool is not Federal Information Processing Standard (FIPS) compliant. When you install LIP on a FIPS 140-2 compliant Site Director, you must uninstall LIP after you add the additional languages.
Table 1. Network engines and applications supported by LIP

Type of network engine/application

Supported product

Locale set by *

Metasys server software

Application and Data Server (ADS and ADS-Lite)

Localization window

Extended Application and Data Server (ADX)

Localization window

Open Application Server (OAS) Localization window

Metasys Advanced Reporting System

Internet browser

NAE85/LCS85/NIE89 Site Management Portal Localization window

Metasys software applications

Graphic Generation Tool (GGT)

Operating system

Metasys Export Utility

Operating system

Metasys UI or Johnson Controls System Configuration Tool (JCT)

Localization window

System Configuration Tool (SCT)

Localization window

Metasys network engines

NAE35

NIE55

Localization window

NAE45

NIE85

Localization window

NAE45-Lite

NIE59

Localization window

NAE55

NIE49

Localization window

LCS85

NIE39

Localization window

NCE25

NIE29

Localization window

SNC16, SNC25, SNE10, SNE11, SNE22

Localization window

Note: The LIP does not change the locale settings for all the software. For products not covered in this guide, check your Internet browser, or your operating system.