Changing the locale for a language on a network engine - Metasys - LIT-12011349 - Software Application - Language Installation Program - 13.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
13.0
Revision date
2024-02-20
Product status
Active
Language
English

About this task

Important: If you are connected directly to the engine, make sure you log out and close the web browser window before you change the locale for a language for a network engine. Also, make sure all other users log out of the network engine. The engine restarts to complete the language change process.

Procedure

  1. Start the LIP tool.
  2. In the Language Pack(s) location window, verify, or change if necessary the file location of the product's translated language packs. Click OK.
  3. In the Settings menu, select Localization.
  4. In the Select Application list, select an engine. For example, to change the locale for an NAE55 Site Management Portal, select N50 Class Device (See Help for Examples).

    N50 Class devices include the NAE55, NIE59, SNE, and SNC.

  5. To establish communication between the LIP and the engine, complete the credentials in the Metasys Login window.
    Figure 1. Metasys Login screen
    1. In the Connection Type area, click Hostname or IP Address.
    2. If you select IP Address, enter the IP address of the site director.
    3. In the Device Hostname (SiteDirector:DeviceName) field, enter the name of the Site Director followed by the network engine name using the following case sensitive format: <Site Director Hostname:Network Engine Hostname>.
    4. In the Username and Password fields, type valid administrator login credentials for the engine.
    5. Click Test Login. This process may take over a minute to complete. If you receive an error message during the connection process, refer to the Troubleshooting section in the Language Installation Program Help (LIT-12011349).

    When the connection is made the LIP fields refresh to reflect the connection to the engine. The following user message appears:

    • Warning - The NxE will restart automatically after the LIP applies the requested language change.
  6. Click OK.
    Note: If an engine restart is not possible at this time, do not proceed to the next step.
  7. In the Language area, select a language.
  8. In the Country Locale area, click Change. This following message appears:

    NxE is now restarting. Depending on the engine, the restart can take from 5 to 20 minutes to complete

  9. Click OK to clear the message. The Results window displays the progress of the request change and the system saves the results to a text file called log.txt. To open the results, click the Results hyperlink. If the Results window contains an error message, refer to the Troubleshooting section in the Language Installation Program Help (LIT-12011349).
  10. In the Language and Country Locale area, in the In use field, verify that the details are correct.
    If you selected the Metasys server and want to add additional languages, see Adding a language.