LIP process flowcharts - Metasys - LIT-12011349 - Software Application - Language Installation Program - 12.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

Figure 1 outlines how to use LIP to change the default language on an ADS, ADX, or OAS computer that has Metasys Advanced Reporting System installed.

Note:
  • For a split ADX, perform all LIP operations locally on the web or application server computer. You cannot access the web or application server remotely with the LIP. Also, do not run the LIP on the database server computer.
  • OAS does not support Metasys Advanced Reporting System.
Figure 1. LIP selection process - Metasys Advanced Reporting System and Metasys UI