LIP internationalization window - Metasys - LIT-12011349 - Software Application - Language Installation Program - 12.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

Figure 1 shows the components of the main LIP screen. For information on each component, see Table 1.

Figure 1. LIP internationalization window: example uses an ADS/ADX product

Table 1. LIP internationalization window options
Callout Description

1

Menu bar options:

Settings: Language Files Location, Internationalization, Localization, Translate LIP

Help: Info, About, Device Examples

2

Language Pack path: location previously selected where the LIP tool looks for translated language files.

3

Select Application: select a product from the list. For remote applications, the list contains all options. For local applications, the list contains only those applications that are currently installed on the computer.

4

Install Path: the folder where Metasys products are installed.

5

Languages in use: the number of languages currently installed for the selected product.

6

Default Language: lists the default languages that you downloaded and unzipped to your computer. The In Use field indicates which language is currently installed for the product you selected. If a product is not selected, this field displays xx_YY.

7

Additional Languages: lists all languages available in the languages folder that you can add to the product in the Available column. They include those downloaded and unzipped to your computer. The In Use field indicates which additional language is currently installed for the product you selected. If the Additional Language column is gray, you cannot select additional languages for the product.

8

Results: captures results of LIP actions. This pane is empty each time you start the LIP. Click the Results hyperlink to view the results of all LIP actions from the time you installed the LIP. The log file opens in the default text editor. Locate the file in the following two possible locations:

C:\Program Files\Johnson Controls\LIP\log.txt

C:\Program Files (x86)\Johnson Controls\LIP\log.txt