Johnson Controls System Configuration Tool (JCT) - Metasys - LIT-12011349 - Software Application - Language Installation Program - 12.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

When you add an additional language for the JCT, you need to restart the JCT server. Be sure to plan for this temporary downtime because all users currently logged in to the JCT are logged out during this process.

You can customize the language that displays in the JCT for each user by using the Tools > User Profile menu. If a language is not selected from the User Profile menu, the Metasys UI uses the same default language as the server.

Verify that any languages that you want to view on the JCT are also installed on the Windows Server.

After you have added additional languages for the Metasys UI, the application pool for Metasys UI is automatically recycled.