Summary of changes - Metasys - LIT-12011349 - Software Application - Language Installation Program - 12.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English
The following information is new or revised:
  • Removed support for SQL Server® 2014.
  • Removed support for Windows® 8.1.
  • Replaced references to Metasys UI Offline with Johnson Controls System Configuration Tool (JCT) throughout this document, as this tool was rebranded.
  • Removed support for Metasys Open Data Server (ODS)
  • Removed support for Energy Essentials
  • The LIP tool is not Federal Information Processing Standard (FIPS) compliant. When you install LIP on a FIPS 140-2 compliant Site Director, you must uninstall LIP after you add the additional languages.