Starting the LIP - Metasys - LIT-12011349 - Software Application - Language Installation Program - 12.0

Language Installation Program Help

Brand
Metasys
Product name
Language Installation Program
Document type
User Guide
Document number
LIT-12011349
Version
12.0
Revision date
2022-05-20
Product status
Active
Language
English

Procedure

  1. Right-click the LIP icon, and click Run as Administrator.
  2. In the Language Pack(s) location window, click Browse and navigate to the location of the compatible language pack files. This location must be on the local drive, or a mapped network drive with an assigned drive letter. Do not use Windows UNC locations. Click OK to save the location.
    If you did not download the language pack files, click the Johnson Controls Intranet Site link in the Language Pack(s) location window, and refer to the Language Installation Program Installation Guide (LIT-12011793) .