LNS LN -Monitor Plug-in - Metasys - LIT-12011298 - Field Device - Variable Air Volume and Temperature Controller - LN Series Variable Air Volume Controller

LN VAV Box Controllers Product Bulletin

Product
Document number
LIT-12011298
Version
. .
Revision date
2020-06-15

The monitoring plug-in is a graphical interface that monitors all device parameters including inputs, outputs, alarms, and device status. You do not need to create any graphics pages, and you can launch it from any Graphical User Interface (GUI) that supports plug-in applications. Graphics dynamically adapt to the configuration of the device as well as monitoring of real-time values. You can use the LN -Monitor plug-in when the LN -VAVLF-2 or LN -VAVLN-2 controllers are not connected to the larger Metasys® network.