Configure schedules and holidays - Metasys - LIT-12011298 - Field Device - Variable Air Volume and Temperature Controller - LN Series Variable Air Volume Controller

LN VAV Box Controllers Product Bulletin

Product
Document type
Product Bulletin
Document number
LIT-12011298
Version
. .
Revision date
2020-06-15
Configure the controller’s built-in schedules and holidays directly from the LN GPI plug-in with an easy-to-use point, drag, and click interface. It features a weekly schedule for regular repeating events by time-of-day and day-of-week, while a holiday schedule is available to define events for specific days. The LN-VAV04060-0 controller allows you to complete the following actions:
  • Configure schedules using a graphical slider.
  • Copy and paste entries, and duplicate a schedule entry for Monday to Friday.
  • Set exceptions to a schedule, such as holidays, with Special Events.
  • Set holidays for recurring events such as, for example, the third Thursday of a given month.
  • Create a schedule as an effective period during which the schedule is active.
  • Create a schedule that provides Next State and Time to Next State — ideal for use with programming functions such as Optimum Start and morning Warm Up.