LN Series Communicating Sensors - Metasys - LIT-12011298 - Field Device - LN Series Variable Air Volume Controller - Variable Air Volume and Temperature Controller

LN VAV Box Controllers Product Bulletin

Product
Document type
Product Bulletin
Document number
LIT-12011298
Version
. .
Revision date
2020-06-15

The LN Series Communicating Sensors feature a backlit display and graphical menus. You can use the sensors as a handheld tool to start VAV commissioning immediately after you install it. Use the sensor to select the appropriate VAV controller application for the VAV box configuration in use, to perform air balancing of the system without requiring an on-site controls engineer, and to troubleshoot the system. The LN Communicating Sensor capabilities include a Leaf icon that displays the efficiency of your setpoints.

Figure 1. Leaf icon
The LN Series Communicating Sensors are available in two versions:
  • The LN-SVSEN-0 room temperature sensor with backlight display, graphic menus, and Leaf icon.
  • The LN-SVSENH-0 room temperature and humidity sensor with backlight display, graphic menus, and Leaf icon.
Figure 2. LN Series Communicating Sensor