Remote site communication - Metasys - LIT-12011549 - Supervisory Device - LCS85 Controller - 13.0

LCS85 Product Bulletin

Product
Controls > Supervisory Controls > LCS85 Controller
Document number
LIT-12011549
Version
13.0
Revision date
2023-09-06
Product status
Active

Remote access to the LCS85 SMP UI or Metasys UI can be established from any computer on the building network, or set up over the Internet using an Internet service provider (ISP) line to the LCS85 Ethernet port. Local access is also possible directly from the LCS85 server.