LonWorks network - Metasys - LIT-12011549 - Supervisory Device - LCS85 Controller - 13.0

LCS85 Product Bulletin

Product
Controls > Supervisory Controls > LCS85 Controller
Document number
LIT-12011549
Version
13.0
Revision date
2023-09-06
Product status
Active

The LCS85 supervises LonWorks devices using LonMark® guidelines. The LonWorks network interface supports all LonMark certified devices, including Johnson Controls® devices, such as the LN Series Controllers, the NexSys controller line, including the LonWorks programmable FSC.