Automation level communication - Metasys - LIT-12011549 - Supervisory Device - LCS85 Controller - 13.0

LCS85 Product Bulletin

Product
Controls > Supervisory Controls > LCS85 Controller
Document number
LIT-12011549
Version
13.0
Revision date
2023-09-06
Product status
Active

The LCS85 communicates internal system data using peer-to-peer messaging over the IP Ethernet network. Each LCS85 shares data and has access to information on the other LCS85s connected on the network, which enables coordination and control of the entire building management system.