Flat LonWorks system - Metasys - LIT-12011549 - Supervisory Device - LCS85 Controller - 13.0

LCS85 Product Bulletin

Product
Controls > Supervisory Controls > LCS85 Controller
Document number
LIT-12011549
Version
13.0
Revision date
2023-09-06
Product status
Active

The LCS85 integrates into the LonWorks network using an open-architecture flat LonWorks system. In a basic flat LonWorks system, the network is managed by a single, LonWorks Computer running an LNS-based, or IzOT-based network management tool, such as LN Builder or LonMaker.

The LCS85 communicates over the TCP/IP network with LonWorks IP routers using the ANSI/CTA-852 protocol standard. In a flat LonWorks system, a Configuration Server is necessary to manage the membership of the IP-852 channel so that all devices can route traffic to one another.

Note: The designated Configuration Server must be either a Loytec L-IP router or an Echelon Configuration Server. See Ordering information for ordering information.

The following figure shows a complex flat LonWorks system setup with the Configuration Server positioned at IP address 10.100.5.1.

Figure 1. Flat LonWorks System

Refer to the LonWorks® Network Integration with Network Engines and LCS Technical Bulletin (LIT-1201668) for more information on the LonWorks network and flat LonWorks system.