Object support - Metasys - LIT-12011549 - Supervisory Device - LCS85 Controller - 12.0

LCS85 Product Bulletin

Product
Controls > Supervisory Controls > LCS85 Controller
Document type
Product Bulletin
Document number
LIT-12011549
Version
12.0
Revision date
2022-05-04
Product status
Active

The LCS85 supports 10,000 objects on the LonWorks network, but is capable of supporting up to 25,000 objects if you order the 15,000-object software upgrade for the LCS85 (MS-15KUPG-0). If you upgrade your system, the maximum amount of permanent status objects is 11,000. Permanent status objects include COV Trends (not sample-based), Alarm Extensions, Global Data Shares, and other objects involved in logic or other Metasys features. For a complete list of permanent status objects, refer to the LonWorks® Network Integration with NAE and LCS Technical Bulletin (LIT-1201668) .