BACnet protocol - Metasys - LIT-12011549 - Supervisory Device - LCS85 Controller - 12.0

LCS85 Product Bulletin

Product
Controls > Supervisory Controls > LCS85 Controller
Document type
Product Bulletin
Document number
LIT-12011549
Version
12.0
Revision date
2022-05-04
Product status
Active

Although the primary function of the LCS85 is to supervise many LonWorks devices over an IP network, it can also integrate devices through BACnet/IP communications. For example, a preferred metering device that uses BACnet/IP could be used with the Demand Limiting Load Rolling (DLLR) feature to shed appropriate loads on the LonWorks network.